Technical FAQs

Ask a Question

What is the replacement coil cover for 8536SC** starter?<br /><br />** followed by (1) letter and (1) or (2) numbers; i.e. 8536SCG3, 8536SAG12

Issue:
What is the replacement coil cover for 8536SC** starter?  ** is followed by (1) letter (enclosure type) and (1) or (2) numbers - For example - 8536SCG3, 8536SAG12, etc. 

Product Line:
8502, 8536 Nema Type S Starter

Environment:
North American Products

Resolution:
31127-013-01 is the cover only. 
The cover is secured by (2x) 21937-14341 mounting screws. Cover does not include nameplate and the nameplate not available for safety reasons.
Was this helpful?
What can we do to improve the information ?