Technical FAQs

Ask a Question

What is the coil consumption or burden for the Tesys LC*D** contactors?<br /><br />* 1 or 2<br />** 09 through 38

Issue:
Coil consumption or burden for the Tesys LC1D/2D contactors from 9A - 38A

Product Line: 
Contactors and Starters - IEC

Environment:
North American Products

Resolution:
All AC coils for the LC1D09 through LC1D38 3-pole contactors ( including ring tongue, quick connect and spring terminal versions ) have an inrush of 70 volt-amps for either 50 or 60 Hertz applications, and a sealed value of 7 volt-amps for 50Hertz applications or 7.5 volt-amps for 60 Hertz applications.
Was this helpful?
What can we do to improve the information ?