Technical FAQs

Ask a Question

How many fuse clips are provided with the Class 9999 Type S* fuse clip kits?

Issue:
Number of clips in a kit

Product Line:
Class 8940 Class 9422 Class 9999 Class Disconnect Switches

Environment:
Flange Mounted and Cable Operated Disconnect spare parts

Resolution:
These kits are supplied with 3 line side and 3 load side fuse clips and necessary mounting hardware.

***9999S5 and 9999SJ5 were obsoleted Dec 2018.
 
Was this helpful?
What can we do to improve the information ?