Technical FAQs

Ask a Question

What is the part number for Hand-Off-Auto (HOA) Insta-Kit for the LE1D and LE2D metallic enclosed Tesys D-Line contactors or starters?

Issue:
Hand Off Auto kit needed for an enclosed LE*D, IEC starter

Product Line:
LE1D Instakit IEC enclosed starters

Environment:
North American Products

Cause:
Hand off auto is required in the application

Resolution:
LA9CA06ET is the part number for the Hand-Off-Auto (HOA) selector switch Insta-Kits.  This is for field installation.
Was this helpful?
What can we do to improve the information ?