Technical FAQs

Ask a Question

What is the difference between a STR25DP and a STR25DE trip unit for the Compact CK breaker?

Product Line:
Circuit Breakers

Electrical Distribution Equipment

The difference is the adjustments for long time.  The STR25DP is adjustable from
0.8 to 1 times rating plug (Io) value.  The rating plug can be changed.  The STR25DE is adjustable from 0.4 to 1 times the sensor (In) value.  The sensor cannot be changed.
Was this helpful?
What can we do to improve the information ?