Technical FAQs

Ask a Question

What is the coil burden for the standard DC control coil for the LC*D09__ through LC*D38__ TeSys contactors?

Issue:
LC*D09-38 coil consumption

Product Line:
Contactors and Overload Relays

Environment:
TeSys™ D Contactors and Overload Relays

Resolution:
The standard DC coil is 5.4 watts of consumption.
Was this helpful?
What can we do to improve the information ?