Technical FAQs

Ask a Question

What are the acceptable mounting positions for the Class 8910 Type DP__, Type DPA__ or Type SYD__ definite purpose contactors?

Issue:
8910 mounting options

Product Line:
Class 8910 Definite Purpose Contactors

Environment:
Types DP, DPA

Resolution:
These devices are designed to be mounted on the normal vertical plane only. Any deviation from this mounting position could result in improper operation, i.e. failure to open and/or close.
Was this helpful?
What can we do to improve the information ?