Technical FAQs

Ask a Question

What is needed to interlock two LC1D80 or two LC1D95 contactors for a reversing application?

Issue:
Mechanical and electrical interlock for LC1D80** and LC1D95**

Product Line:
Tesys D line Contactors

Environment:
Contactor Accessories

Resolution:
For LC1D80 or LC1D95 with AC coils
LA9D4002 mechanical interlock with integral electrical interlocking
LA9D50978 mechanical interlock without electrical interlocking
LA9D8069 - 3 pole power connectors***

For LC1D80 or LC1D95 with DC coils
LA9D8002 mechanical interlock with integral electrical interlocking
LA9D80978 mechanical interlock without electrical interlocking
LA9D8069 - 3 pole power connectors***

***Connectors for 4 pole contactor set is LA9D8070.
Was this helpful?
What can we do to improve the information ?