Technical FAQs

Ask a Question

What is the difference between the GV2MC01 and the GV2MC02 enclosures?

Product Line:
GV Manual Motor Starters and Protectors
The GV2MC01 has an IP41 rating ( similar to Nema Type 1 ), whereas the GV2MC02 has an IP55 rating (similar to the Nema Type 12 ).

Was this helpful?
What can we do to improve the information ?