Browse FAQs

What is the Temperature Threshold at which the Cooling Fan of Altistart 48 Soft Starter start and stop is controlled?

Published date: 11 August 2019

The Temperature Thresholds at which the Cooling Fan of Altistart 48 Soft Starter start and stop is controlled are as follows:

1. Start – Heatsink Temperature > 50°C.
 
2. Stop – Heatsink Temperature < 40°C.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.