Technical FAQs

Ask a Question

What is the amperage rating on Power Distribution Block catalog number 9080LBA361104?

Issue:
Maximum current value for 9080LBA361104

Product Line:
9080 Type LB, PDB, Power distribution blocks

Environment:
n/a

Cause:
N/A

Resolution:
These units are rated for 115 amps with copper wire and 90 amps with aluminum wire.  Max 600 volts.

9080LBA361104
9080LBA261104
9080LBA161104
9080LBA361101
9080LBA261101
9080LBA161101
Was this helpful?
What can we do to improve the information ?