Browse FAQs

Is Ethernet communication available on ATS48 or ATS22 solid state softstarts?

Published date: 10 August 2019

Issue:
Needs Ethernet communication  on the ATS48 or ATS22 solid state softstarts

Product Line:
ATS22, ATS48

Environment:
All

Cause:
NA

Resolution:
The ATS22 and ATS48 only support Modbus communication protocol.
Use a Gateway for Modbus - Ethernet IP conversion.
Consider the EGX150 - Link150 Ethernet Gateway or a device from a 3rd party such as ProSoft or AnyBus.
Please be aware that you cannot do I/O scanning on the ATS48 or the ATS22 soft starter.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.