Technical FAQs

Ask a Question

Do the Class 9422T fusible disconnect switches include Class R fuse rejection clips?

Issue:
Class R fuse rejection clips on fusible disconnect

Product Line:
9422 Disconnect Switches Op Mech

Environment:
Flange Mounted and Cable Operated
 
Resolution:
Class R fuse clip kits are ordered separately.
Was this helpful?
What can we do to improve the information ?