Technical FAQs

Ask a Question

Are the IEC D-Line contactors SEMI F47 compliant?

Issue: 
 Identifying D line contactors compliance

Product Line:
Tesys D contactors

Environment:
Products sold and used in the United States
 
Cause:
 SEMI F47 compliance required
 
Resolution:
 
D-Line contactors with AC coils are not SEMI F47 compliant.

D-Line contactors with DC coils are SEMI F47 compliant and perfect for EMO contactor applications. Additionally, the addition of an overload relay makes them SEMI F47 compliant motor starters.


 
Was this helpful?
What can we do to improve the information ?