Technical FAQs

Ask a Question

What is the IP rating for 22mm Push Buttons XB4 and XB5?

Issue:
Clarify the 22mm operator IP rating

Product Line:
Harmony XB4/XB5 22mm push button

Environment:
US Product

Cause:
Product Specification

Resolution:
As of 2017, all of the XB4 and XB5 push buttons are rated IP66, IP67, IP69, and IP69K or UL Type 4X. 
 
Was this helpful?
What can we do to improve the information ?