Technical FAQs

Ask a Question

Can the LUB32 use the smaller (less than 12 amps) control units?

Product Line:
Tesys U Line Motor Starters
 Yes, it can.
That being said the LUB12 cannot use the larger (greater than 12 amps) control modules. 
Was this helpful?
What can we do to improve the information ?