Technical FAQs

Ask a Question

How do I select the correct Smart-UPS XL battery pack for my Legacy Smart-UPS?


Issue:

How do I select the correct Smart-UPS XL battery pack for my Legacy Smart-UPS?

Product Line:  

Smart-UPS

Environment:

SU and SUA "XL" models, All Serial Numbers

Cause:

"XL" models allow for the use of external batteries to extend runtime.

Resolution:

"APC manufactures a wide VA range of Smart-UPS products. Some of these models
have large, more robust battery chargers. This allows the user to add
additional external battery packs to the Smart-UPS. This feature increases the
runtime when operating on battery. It is important to understand which
Smart-UPS will function with the appropriate external battery pack.

*All Smart-UPS with the extended run feature, will have the letters ""XL"" in the part number. The only exceptions would include the SU3000NET, SU3000TNET and the SU3000RMNET.

The chart below contains all current production Smart-UPS, as well as recently
discontinued Smart-UPS, which support an additional battery pack, and the battery
packs with which they are compatible.

UPS Model

Battery Pack Model

SU700XLNET (disc.)

SU24XLBP or UXBP24

SUA750XL

SUA24XLBP (will work w/ SU24XLBP and UXBP24, but they are different colors)

SU1000XLNET (disc.)

SU24XLBP or UXBP24

SUA1000XL

SUA24XLBP (will work w/ SU24XLBP and UXBP24, but they are different colors)

SU2200XLNET

SU48XLBP or UXBP48

SU1400RMXL3U

SU24RMXLBP2U only

SU1400RMXLNET (disc.)

SU48RMXLBP or UXBP48 (not rack-mountable)

SU2200RMXLNET (disc.)

SU48RMXLBP or UXBP48 (not rack-mountable)

SU2200RMXL3U

SU48RMXLBP3U only

SU3000RMXL3U

SU48RMXLBP3U only

SU2200XLTNET

SU48XLBP or UXBP48

SU2200RMXLTNET

SU48RMXLBP or UXBP48 (not rack-mountable)

SU3000NET

SU48BP only

SU3000TNET

SU48BP only

SU3000RMNET

SU48BP only (not rack-mountable)

SU5000RMXLT5U

SU48R3XLBP only

"
Was this helpful?
What can we do to improve the information ?