Browse FAQs

Thermal Dissipation of PowerStack 250 and 450

Published date: 05 June 2019

"The following table gives typical thermal dissipation as a function of mode of

operation. The models listed below are 120V and 230V versions of PowerStack

250 and 450. On-battery thermal dissipation is given at full rated load over

the entire battery discharge period. Note that on-battery thermal dissipation

is limited in duration according to available battery capacity and output

loading.


 
Model Operating On-line
Watts [BTU/Hr]
Operating On-battery
Watts [BTU/Hr]
250 16[55] 35[120]
450 10[34] 75[256]
"

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.