Technical FAQs

Ask a Question

What is the FM Water Flow Switch Alarms description?

Issue: FM Water Flow Switch Alarm
 
Product line: FM
 
Environment: Data Center Cooling
 
Cause:
 
Resolution:
Here are the conditions for producing a flow switch alarm:

Note that the flow switch opens when there is no flow.

If you have selected a flow switch = MC/CW
If the flow switch is open and the MC/CW valve is a 3 way valve then an alarm will be generated.
If the flow switch is open and the MC/CW valve is a 2 way valve and the valve is open more than 30% then an alarm is generated.

If you have selected a flow switch = DX/ECON
If the flow switch is open and [the coil configuration = ECON or the water regulation valve = 3 way or (the water regulation valve = 2 way and the water regulation valve is open more than 30%)] then an alarm is generated.
 
Was this helpful?
What can we do to improve the information ?