Browse FAQs

How long are the intake and exhaust hoses on the ACPA4000?

Published date: 16 May 2019

Issue: The Length of the intake and exhaust ducts on the ACPA4000
 
Product line: ACPA4000
 
Environment: Data Center Cooling
 
Cause:
 
Resolution:
The exhaust hose is 10 FT X 8 IN and yes you may have them ducted through a wall. The key point here is that the hot air still needs a way to escape so that it is not recycled through the unit. Please view Application Note 109. It applies to the ACSC10x, but the same rules apply for ducting the condenser section.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.