Browse FAQs

Why doesn't my flow switch shut my Legacy AC down?

Published date: 16 May 2019

Issue: DG5 wiring the flow switch
 
Product line: DG5
 
Environment: Data Center Cooling
 
Cause:
 
Resolution:
This issue is the DG5 Controller is not changing the state of the water flow switch, which does not shut the AC unit down. The water flow switch is wired into Digital Input 7 is set to WtrFl2

The solution to this is to go through Factory Setup 1, I/O setup. Set Digital Input 7 (pg4) to WtrFl3.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.