Browse FAQs

When do the cooling fans on the ATV212 drives come on?

Published date: 19 August 2019

Issue:
Wondering when the cooling fans on the ATV212 drives come on?

Product Line:
Altivar 212

Environment:
All

Cause:
Fan control strategy

Resolution:
The fan starts when the drive is in RUN state.
The fan stops after the STOP command (with a time delay in relation to the thermal state).

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.