Technical FAQs

Ask a Question

When programming the ATS48 analog output for motor current scaled?

Issue:
When programming the ATS48 analog output for motor current, AO=OCr, is the scaling parameter ASC a percentage based on the motor current parameter In or based on the nameplate current rating of the specific ATS48?
 
Product Line:
Altistart 48, ATS48
 
 Environment:
 All
 
Cause:
Programming the ATS48 analog output for motor current.
 
Resolution:
It is based on the motor current programmed into In.  It is adjustable from 50 to 500% of the In value.

 
Was this helpful?
What can we do to improve the information ?