Technical FAQs

Ask a Question

What is the command word for the ATS22 soft starters for network communication?

Issue:
What is the command word for the ATS22 soft starters?

Product Line:
Altistart ATS22

Environment:
All

Cause:
Modbus address for ATS22

Resolution:
The command word address for the ATS22 soft starter is 752.
The ETA status word address for the ATS22 soft starter is 256

See the attached PDF document for the Command word and the ETA status bit assignments.

Was this helpful?
What can we do to improve the information ?