Technical FAQs

Ask a Question

When do the ATS48 internal cooling fans run?

Issue:
When do the ATS48 internal cooling fans run?

Product Line:
Altistart 48

Environment:
All

Cause:
NA

Resolution:
ATS48D17Y and ATS48D22Y do not have fans.  All other models do have fans.
The fans will operate when the heatsink temperature is greater than 50C.
The fans will stop operating when the heatsink temperature drops below 40C.


 
Was this helpful?
What can we do to improve the information ?