Technical FAQs

Ask a Question

Video: What can cause connection in progress issue on HMI keypad VW3A1101 with ATV212 drive?

Issue:
Connection in progress issue on HMI keypad VW3A1101, with ATV212 drive
Product Line:
Altivar 212

Environment:
All 

Cause:
In most cases the issue is because the baud rate and parity settings of the HMI modbus has been altered.

Resolution:
Verify the following parameters using built in display.
F800=1 (Baud rate) 1= 19.2K
F801=1 (Parity) 1= Even parity

Also, the keypad Flash must be V1.1IE29 or higher.  
Also try swapping out the control terminal block with a known good one that has the F, R RES wires connected to it. 

Power cycle once changes are made.

In other cases, a power supply issue where the +10V source PP and +24V source P24 may have issues or shorting.

Was this helpful?
What can we do to improve the information ?