Technical FAQs

Ask a Question

With the ATV212, can the drive's programming be saved to the HMI keypad (VW3A1101) and transferred to another ATV212?

Issue:
With the ATV212, can the drive's programming be saved to the HMI keypad (VW3A1101) and transferred to another ATV212?

Product Line:
Altivar 212

Environment:
All

Cause:
N/A

Resolution:
No.  With the ATV212, the programming cannot be saved to any of the keypads available.  

Programming can be saved by three methods:
- in the drive by setting parameter tYP = 7
- in the Multiloader tool
- by using SoMove software, downloading the ATV212 DTM File, and using the TCSMCNAM3M002P - SoMove cable
Was this helpful?
What can we do to improve the information ?