Technical FAQs

Ask a Question

ATV212 How can I get a run status ?

Issue:
ATV212 -needs a run status .

Product line:
Altivar 212  

Environment:
All models, all serial numbers   

Cause:
The customer wants a signal from the drive indicating that the motor is running

Resolution:
Wire to RYA and RYC relay and program F130 to 14 (drive running).   The relay will close if a run command is issued and there are no faults.
Was this helpful?
What can we do to improve the information ?