Technical FAQs

Ask a Question

What is a good source of information for the ATS48 soft start?

Issue:
Information is needed to facilitate installation and programming.

Product line:
Altistart ATS48

Environment:
All models, all serial numbers

Cause:
None

Resolution:
Instruction Bulletin, S1A37491, includes information for installing and programming the ATS48.
Instruction Bulletin, 30072-451-28, is a Maintenance and Repair manual.

Use this URL to get to the ATS48 product page:
https://www.schneider-electric.com/en/product-range/689-altistart-48/
Was this helpful?
What can we do to improve the information ?