Technical FAQs

Ask a Question

How to adjust the torque boost or voltage boost on the ATS48 soft starter?

Issue:
How do you adjust the toque boost or voltage boost on the ATS48 soft starter?

Product Line:
Altistart ATS48

Environment:
All

Cause:
Boost to torque

Resolution:
SET Menu:
T90  set to desired torque setting.  Example 100% would mean 100% starting torque at start up.
Can bump up the value as needed.
Was this helpful?
What can we do to improve the information ?