Technical FAQs

Ask a Question

Video: How to lock/unlock the ATV212 drive?

Issue:
How to lock the ATV212 drive so that the parameters cannot be altered?

Product Line: 
Altivar 212  ATV212

Resolution: 
From main menu and enter.
Arrow down to F--- and enter.
Go up to F700.
F700 : 0 is unlocked.
F700: 1 is locked.

Drive will not allow any programming changes unless this parameter is diabled.

Was this helpful?
What can we do to improve the information ?