Technical FAQs

Ask a Question

What are the secondary-injection test kits for Micrologic circuit breakers?


Product Line:
Legacy, Powerpact, and Masterpact circuit breakers

Resolution:
The secondary injection test kit for Legacy Micrologic (Micrologic Series B) breakers is the UTS3.
The Full Function Test Kit  (FFTK) for Powerpact M, P, R frame and Masterpact circuit breakers with electronic or Micrologic trip units is S33595.
The Hand Held Test Kit (HHTK) for Powerpact M, P, R frame and Masterpact circuit breakers with electronic or Micrologic trip units is S33594.
The UTA tester for testing Powerpact H, J, Lcircuit breakers is STRV00910.
The Pocket Tester for testing Powerpact H, J, Lcircuit breakers is S434206.
The Universal Test Kit for testing Legacy Micrologic (Micrologic Series B) trip units is UTS3.
The test kit for testing Masterpact and Compact circuit breakers with STR trip units is 55391.
 
Was this helpful?
What can we do to improve the information ?