Technical FAQs

Ask a Question

What is the part number of the Sepam software and cable to attach to the Sepam for programming via the software?

Issue
Distributor would like the part number for the Sepam software and cable

Product Line
Sepam relays

Environment
Part number

Resolution
The software and cable are sold as a kit under the part number SFT2841KIT.

The individual part number for the cable is CCA783.
The software can be downloaded separately here: FA180051

Was this helpful?
What can we do to improve the information ?