Technical FAQs

Ask a Question

What is the minimum version of the Unitelway driver required to use the USB cable (TSXPCX3030 or TSXCUSB485)?

Issue: 
Minimum version of the Unitelway driver required to use the USB cable (TSXPCX3030 or TSXCUSB485)

Product Line:
TSXCUSB485, Unitelway

Resolution:
To use the USB cable (TSXCUSB485 or TSXPCX3030) your Unitelway must be Version 1.8 or later.


Was this helpful?
What can we do to improve the information ?