Technical FAQs

Ask a Question

How do we include the Editor project (.VDZ backup project file) in the HMI with Vijeo Designer V6.2?

Issue
How do we include the Editor project (.VDZ backup project file) in the HMI with Vijeo Designer V6.2?

Product Line
Vijeo Designer v6.2

Environment
Magelis HMI Configuration software in Windows

Resolution
Under the download section, set the Include Editor Project setting to Enable.  By default this option is disabled.
Go to Data location and set the Data Files / Forms Drive to where you want the .VDZ backup file to be stored.  You can select between Main (Internal memory), Secondary (CF or SD Card depending on model) and Optional (USB memory stick) drives depending on the HMI model.

If you choose Main, to allow Vijeo Designer Data Manager to access the HMI in the future:
1. In the Project Navigator, select the Environment->Security node.
2. In the Property Inspector window, next to Download Security, choose either "Anonymous", or "Use Security"

Was this helpful?
What can we do to improve the information ?