Technical FAQs

Ask a Question

In Vijeo Designer, is there a way to cross reference all variables and where it is being used?

Issue: 
How to cross reference all variables and where it is being used in Vijeo Designer.

Product Line:
Vijeo Designer

Resolution:
Yes, you can cross reference all variables used in Vijeo Designer. Below is the instructions on how to get the report:
1 - Select (highlight) the variable node

2 - Goto the Report Menu and select Variables..

3 - Select Yes

4 - Change the Variable Report to "cross reference all variables by name" and select OK

5 - Then the list will be generated.


Was this helpful?
What can we do to improve the information ?