Technical FAQs

Ask a Question

Why am I getting an error message: "PLC return error code FDH-83,80H" when communicating between a Magelis and a Unity Quantum PLC?

Issue: 
Getting an error message: "PLC return error code FDH-83,80H" when communicating between a Magelis and a Unity Quantum PLC


Product Line:
Vijeo Designer, Quantum PLC


Resolution:
The error message is due to the Magelis reading the discrete/analog inputs as %I or %IW from the Unity Quantum. You will need to delete the tags and link to the Unity database file. Then re-link the tags back into Vijeo Designer and check the box to "force IO to unlocated variables". Or convert all of the input variables to memory bits and words.

 
Was this helpful?
What can we do to improve the information ?