Technical FAQs

Ask a Question

How do you wire a DC sink and DC source input on a Twido input module?

Issue:
Wiring Twido Modules for sink and source.

Product Line:
Twido

Environment:
TwidoSoft, TwidoSuite

Cause: Product not working correctly due to wiring.


Resolution:

See wiring recommendation below for connection of Source / Sink device(s) to a Twido input module:


Note: The Twido line is obsolete and has been replaced with the M221 product line.
Was this helpful?
What can we do to improve the information ?