Browse FAQs

What could cause 'error during connect' when trying to connect to a Premium processor using Unity Pro?

Published date: 12 September 2018

If you have verified that the communication parameters are correct and are still unable to establish communication over Unitelway or USB, make sure that the backplane has two terminators, terminator A on the left side next to the power supply and terminator B on the right side of the backplane.


Legacy KB System (APS) Data: RESL167666 V1.0, Originally authored by on , Last Edited by on
Related ranges: Unity Pro

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.