Technical FAQs

Ask a Question

How do I switch between Power and State Flow in the ProWORX 32 software?

Issue
Switch between Power and State Flow

Product Line
ProWORX 32

Resolution
Open the Logic Editor Properties and under the Logic tab simply check off the box for State Flow. If this box is not checked off then Power Flow is activated.

Was this helpful?
What can we do to improve the information ?