Technical FAQs

Ask a Question

What programming software is required to support the TSX07 Nano PLC?

Issue
Need to identify the programming software for the TSX07 Nano PLC.

Product line
PL7-07, TSX Nano

Resolution
PL7-07 is required to support the TSX 07 Nano PLC. The part number for a single install is TLXLPL707P40M. Note that this is an obsolete DOS based software. There is no windows based equivalent software.

Was this helpful?
What can we do to improve the information ?