Technical FAQs

Ask a Question

What Advantys NIM's can talk to the ATV31 Altivar Drive and what version are they compatible with?

Issue:   What Advantys NIM's can talk to the ATV31 Altivar Drive and what version are they compatible with?
 
Product Line:   ATV31, Advantys
 
Environment:  All
 
Cause:   Advantys NIM's
 
Resolution:   
The following are the Type of NIM's and part numbers along with the minimum version that is required.


Was this helpful?
What can we do to improve the information ?