Technical FAQs

Ask a Question

Can power flow colors be changed in Unity Pro?

Colors can be changed by editing the *colors.ini files located in the c:\Program Files\Schneider Electric\Unity Pro folder.

  • FBD: FBDclolors.ini
  • IL: ILcolors.ini
  • ST: STcolors.ini
  • LD: LDcolors.ini
  • SFC: SFCcolors.ini
  • 984LL: 984colors.ini
  •  
  • Using Microsoft Paint - Custom Colors, as show below, the code for green would be 0,183,0.

  • Animation Table value field colors can also be changed.
  • Put the mouse focus to the right of the icons in the animation table. Press "Ctrl" and right click for the Color Settings.
NOTE:  There is also a  Tools - Color Settings option in Unity Pro v13.1 or later for the the different programming languages.
 
Was this helpful?
What can we do to improve the information ?