Search FAQs
When a phase is connected to neutral ( N ) terminal, is the RM35UB3N30 protected against this ? If so, how would the unit react on this fault.
Goals and Symptoms
When a phase is connected to neutral ( N ) terminal, is the RM35UB3N30 protected against this ? If so, how would the unit react on this fault.
Facts and Changes
RM35UB3N30 RM35U
Wrong connection
Phase
Neutral
Causes and Fixes
If there is a error in connecting the product , and a phase is connected to the neutral ("N" terminal), there is a risk of destruction.
Legacy KB System (APS) Data: RESL197893 V1.0, Originally authored by LaBe on 02/26/2009, Last Edited by LaBe on 02/26/2009
Related ranges: Zelio Control
Released for:Schneider Electric India
Explore more
Explore more