Technical FAQs

Ask a Question

What are the new Twido I/O module part numbers and what I/O modules do they replace?

Issue:
Twido I/O module cross over from TWD to TM2

Product line:
Twido

Cause:
To give matrix on the old part number for the Twido I/O and give new replacement numbers.

Resolution:

Below is the matrix of the old numbers and the new replacement numbers.


Twido was obsolete 12/31/2016 and was replaced by the M221 family. The M221 will support the TM2 modules and the new TM3 modules in the same configuration but not the TWD modules.
Was this helpful?
What can we do to improve the information ?