Technical FAQs

Ask a Question

What is the communications cable between the Twido minidin and Magelis HMISTU655/855 RJ45 port?

Issue: 
Communications cable to use between the Twido mini din and Magelis HMISTU655/855 RJ45 port


Product Line:
Twido, HMISTU


Resolution:
The communications cable between the Twido PLC and the HMISTU655/855 is the XBTZ9780.

 
Was this helpful?
What can we do to improve the information ?