Technical FAQs

Ask a Question

What is the part number for the Twido TWDLMDA20DRT 13 and 16 pin connectors?

The TWDLMDA20DRT connector part numbers are:
13 pin - TWDFTB2T13 (pack of 2)
16 pin - TWDFTB2T16 (pack of 2)


Note: The Twido PLC line is obsolete and the replacement for it is the M221 product line. For more information on this contact your local Schneider office or local distributor. 
 
Was this helpful?
What can we do to improve the information ?