Technical FAQs

Ask a Question

What is the M340 replacement module for the Compact AS-BDEP-220 module?

Issue:
What is the replacement for the BDEP-220 module

Resolution:
The Compact AS-BDEP-220 module replacement to a M340 module would be the BMXDDI1602.

Note: The Compact line is obsolete and has been replaced by the M340 line. Fore further information on this upgrade you can contact your local distributor or Schneider office. See attachment for an overview of the M340 upgrade.
Was this helpful?
What can we do to improve the information ?