Technical FAQs

Ask a Question

What is the Advantys FTXES01?

Issue:
Software for the Advantys OTB

Product Line:
Advantys OTB

Environment:
Advantys Configurations Software

Cause:
Software that can configure only the Advantys OTB

Resolution:
The Advantys FTXES01 is the Lite version of the Advantys configuration software and it is only for the OTB with the Twido IO and does not require authorization. For the Advantys STB hardware, you will need to install the full package and authorize it part number STBSPU1000.

Note: The Advanty OTB and associated TM2 modules are going obsolete in 2019 and will be replaced with new product in late 2019 early 2020.


Was this helpful?
What can we do to improve the information ?