Technical FAQs

Ask a Question

Can the Magelis XBTGC have a Profibus card added to it?

Issue:
Can a Profibus card be added to a Magelis XBTGC

Product line:
Magelis XBTGC

Environment:
Ecostruxure Operator  Terminal Expert (formally Vijeo Designer)

Cause:
Requirement to add Profibus to the XBTGC and there is no way to do it.

Resolution:

No. The Magelis XBTGC can not have the Profibus card added. Only the GT and GK series can have the Profibus card added.

Was this helpful?
What can we do to improve the information ?